DOCA0036EN-14

Wi-Fi Settings

This table illustrates Wi-Fi settings:

Wi-Fi Only Wi-Fi and 2 Ethernet Switched Ports (1 IP Address for Both Ports)

Use any USB port for temporary access, for example, to configure the Com’X.

For permanent use, the Wi-Fi USB key must be installed outside the enclosure for EMC reasons. Schneider Electric provides accessories to mount the Wi-Fi key outside the enclosure.

NOTICE
Unintended equipment Operation
Do not install the Wi-Fi key inside a metallic enclosure.
Failure to follow these instructions can result in equipment damage.

The Com’X does not enable Point-to-Point connections with other Wi-Fi field devices. Wi-Fi traffic is controlled by the Wi-Fi infrastructure of the site.

**See Wifi Access Point Settingsfor more information.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.