DOCA0036EN-14

Main Meter Measure and Signal Properties

The customized main meter has customized settings for the measure properties of each of the two pulse outputs, and the same signal properties as the standard main meter.

Each pulse output presents the following measure properties:

Field Description
Count element Select a measure element from the list, or select Custom and enter a personalized name into the Custom count element field.
Count unit Select a measure unit from the list, or select Custom and enter a personalized unit into the Custom count unit field.
Pulse weight The pulse counter increases by this value each time a pulse is received. The list is restricted to the values that correspond to the selected meter type.
Upper Range

Defines when the active energy counter rolls back to zero.

Flow Element Select a flow element from the list, or select Custom and enter a personalized name into the Custom flow element field.
Flow unit

Select a flow unit from the list, or select Custom and enter a personalized unit into the Custom flow unit field.

Each contact output presents the following signal properties:

Field Description
Signal element Enter the name of this signal, or accept the default name Status Output n, where n represents the signal number (1 to 4).
Value for 0 Enter the status associated with a value of 0. Default is OFF.
Value for 1 Enter the status associated with a value of 1. Default is ON.

Measurements Table

The measure and signal property selections you make, including customized properties for pulse outputs, are reflected in the measurements table.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.