DOCA0036EN-14

Factory Settings of the Device Measurement Table

Some measurements are selected by default in the device measurement table.
Device Type Measurement
Pulse meter
  • Index
Contactor/Impulse relay
  • Status
  • Run hours
Electric utility meter
  • Active energy
  • Reactive energy
Power meter
  • Active energy
  • Reactive energy
Resistance Temperature Detector (RTD) Temperature
0–10 V/4–20 mA analog sensors Analog value
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.