DOCA0036EN-14

Architecture

From a simple metering installation with one device to large metering systems, the Com’X 210 collects data from any Modbus TCP/Modbus serial line gateway, pulse meter, actuator, and analog sensor.

This graphic shows possible architectures of the Com’X 210:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.