DOCA0036EN-14

Read Device Registers

Read Device Registers allows the Com’X to read Modbus registers from its local and remote devices.

Below are Read Device Registers settings.

Setting Description Options
Device Name Selects a device to read from the list of previously added devices. A device not defined in the device list can be read by entering its Local ID.
Local ID The address (Local ID) of the device that is to be read.

1-255

Default: 1

Starting Register The first register to read. Default: 1000
Number of Registers The number of registers to read.

1-125

Default: 10

Register A column displaying the register numbers.
Value

A column displaying the data stored for each register.

Values retrieved depend on the device connected to the Com’X. Refer to the documentation for the connected device for more information about stored register values.

Data Type Menu for selecting the type of data the registers hold and the format (Decimal, Hexadecimal, Binary, or ASCII) you want returned.

Holding Registers, Input Registers, Output Coils, Input Coils, or Device ID

Default: Holding Registers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.