DOCA0036EN-14

Logged Events

Your device logs events.

The events that are logged are:

Topic Event
Resource

Change in the configuration of:

  • devices
  • publication

Delivery Publication steps and status (unsuccessful or successful)
Activation/deactivation of the periodic publication
Logging Activation/deactivation of the data logging
Security Unsuccessful login
Alarm Low level of GPRS/3G signal
Error detected during the login
Device not communicating
CPU and RAM overuse
Communication interruptions with metering devices
System Time setting modification
Firmware update and status
Boot time

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.