DOCA0036EN-14

Firewall Management

Firewall management allows you to configure network access.

You can configure items such as:

  • Enable or disable ports.
  • Configure port numbers per interface (Eth1, Eth2, WiFi, GPRS/3G), except where noted in Port Settings.
  • Enable upstream network access.
  • Enable Account Lockout policy.

Disabling unused ports (determined by your network selection in Settings > General Settings > Network Settings) can help prevent unauthorized access.

** For default port settings, see Port Settings

Upstream Network Access

This feature allows downstream devices to access servers (such as DNS, SNTP, and SMTP) on the upstream network.

Upstream Network Access is disabled by default. It is recommended to leave this setting disabled unless it is required to publish data or send event messages from downstream clients.

** Port Settings

Account Lockout Policy

Account lockout feature disables a user account when the number of failed login attempts exceeds the set limit within a predetermined time interval. You can configure the following:

  • Enable account lockout ­ Account lockout policy is enabled by default. Select No to disable this feature. It is recommended to keep the Account Lockout feature enabled to secure the device from unauthorized access.

  • Reset account lockout counter (number of attempts) ­ determines the number of invalid login attempts allowed before user account gets disabled. The default is set to 10 attempts.

  • Account lockout duration (minutes) ­ determines amount of time user account remains disabled. The default is set to 15 minutes.

Disabling Account Lockout Policy

NOTE: It is recommended to keep the Account Lockout enabled to better secure the device from unauthorized access.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.