DOCA0036EN-14

Maintenance

Real-time access to maintenance logs allow you to check for excessive denied accesses, unexpected firmware upgrades or unplanned backup restoration.

Configuration Backup

Configuration backup allows recovery of Com'X and device settings.

Firmware

Users can only install firmware signed by Schneider Electric.

** See Logs. See Save the Configuration and Restore the Configuration See Upgrade Firmware

Remote Access from Cloud Services

By default, a Com’X device connected to DSP can be accessed through remote assistance. The Enable remote access from cloud option is enabled (ON) by default. For security reasons it is recommended to disable this feature and enable it only when remote access is required for technical support from Schneider Electric.

Refer to Disabling Remote Access from Cloud Services for additional information.
** See Logs. See Save the Configuration and Restore the Configuration See Upgrade Firmware
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.