DOCA0036EN-14

Metering Device Troubleshooting

There are tips for troubleshooting your metering devices.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must only be installed and serviced by qualified personnel.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462 or applicable local standards.
Failure to follow these instructions will result in death or serious injury.

Digital Input Troubleshooting

This table describes how to solve issues with digital inputs.

Issue Possible Solution
No pulse is received. The digital input LED is not flashing. Bridge the input terminals between the terminal and the 12 V power supply with a short piece of wire to confirm that the LED is working. If the input LED lights up when you bridge the input terminals, the issue is likely with the meter and/or the wiring to the meter.

Check that the pulse output meter is connected to a digital input terminal and the 12 V power supply.

Refer to the Installation Guide for wiring diagrams.

Check that the pulse output device is operating.
No pulse is received. The digital input LED is flashing. Check the digital input number to which the pulse meter is connected.

Analog Input Troubleshooting

This table describes how to solve issues with analog inputs.

Issue Possible Solution
No analog value can be read.

Check that the analog output sensor is connected to the proper terminals.

Refer to the Installation Guide for wiring diagrams.

In the configuration web page, check that the analog input number is set to the correct type of sensor: RTD, 0–10 V, or 4–20 mA.

Possible Logging Errors

This table lists the possible logging errors for the Data log.

Error Code Definition
0 No error detected
19 No valid values are recorded for the logging interval. This is most likely the result of failed communications with the device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.