DOCA0036EN-14

Logging In for the First Time

There are special instructions when you log in to the user interface for the first time.

The web server is a tool for reading and writing data. It controls the state of the system, with full access to all data in your application. You will be prompted to change your password the first time you log in to prevent unauthorized access to the application.

NOTICE
UNAUTHORIZED DATA ACCESS
  • Immediately change the default password to a new, secure password.
  • Do not distribute the password to unauthorized or otherwise unqualified personnel.
Failure to follow these instructions can result in equipment damage.
A secure password should not be shared or distributed to unauthorized personnel. The password should not contain any personal or obvious information.

  1. Log in as the default administrator. 

    Username and password: admin

  2. Read the License Agreement completely.
    NOTE: The Accept button will remain grayed until you scroll to the bottom of the User License Agreement.
  3. Accept the License Agreement.
  4. Enter a new password.

    It must contain:

    • 8 characters

    • 1 uppercase letter

    • 1 numeric digit

    • 1 special character

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.