DOCA0036EN-14

Logging In

You need to log in to access the energy server’s user interface.

If multiple sessions are opened, only the first session can be used to edit parameters. Sessions opened after the first session are read-only.

  1. Select your language.
  2. Type the username and the password.
    NOTE: The username and password are case-sensitive.
  3. Click Connect to be logged in to the configuration web page.
NOTE: HTTPS is enabled by default on the Com’X configuration. The Com’X has an autosigned security certificate. Therefore, connecting to the Com’X interface displays a security message. Before accepting, confirm that communication with the Com’X has been established.

To install a new certificate, see Local Web Server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.