DOCA0036EN-14

Starting the Publication

Publication allows you to send data to the hosted platform at a specified frequency.

If you are publishing data to Energy Operation, you must send the topology to Energy Operation.

After you have configured devices for publishing:

  1. Click the Manual publication button to send data to the hosted platform.
  2. Click the Start periodic publication button to send data to the hosted platform according to the frequency set in Publication settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.