DOCA0036EN-14

Activating the Wi-Fi Access Point

You can configure the USB Wi-Fi key to be used as a temporary communication medium during the commissioning phase.
  1. Click Settings > General Settings > Wi-Fi Access Point Settings.
  2. Click Yes to Enable Wi-Fi access point.
  3. Select the duration in the Session duration drop-down list (Default: 1 hour).
  4. Click Save changes.

    If Session duration is modified during a Wi-Fi access point session, the modification is taken into account at the next session.

    This setting only enables access point mode. To start the Wi-Fi access point mode session, push the Wi-Fi button located near the USB port on the front face. The Wi-Fi button LED flashes green.

    see Accessing Through Wi-Fi Access Point Mode
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.