DOCA0036EN-14

Configuring Advanced Ethernet Settings

You to customize network settings for your specific environment by configuring the advanced Ethernet settings.
NOTICE
Impaired Network Performance
Only qualified workers should modify the advanced Ethernet settings. Such modifications should be performed only after reading about and understanding the advanced Ethernet settings.
Failure to follow these instructions can impair network performance.
  1. Click Settings > Communication > Advanced Ethernet Settings.
  2. Enter the Time to Live.
  3. TCP Keep Alive is enabled by default.
    • enter the keep alive time, or
    • click No to disable TCP Keep Alive.
  4. Click Save changes.

    To return to default values, click Defaults.

** see Advanced Ethernet Settings
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.