DOCA0036EN-14

Configuring the Modbus Gateway

You can configure the Com’X Modbus gateway settings.
NOTICE
Impaired Network Performance
Only qualified workers should modify the Modbus gateway settings. Such modifications should be performed only after reading about and understanding the Modbus gateway settings.
Failure to follow these instructions can impair network performance.
  1. Click Settings > Communication > Modbus Gateway.
  2. Select the required Transmission Mode, Silent Interval Extension, and Delay Between Frames for the serial port.
  3. Select Yes or No to Enable Server Connection Idle Time, Enable Modbus TCP/IP Proxy, and Enable Serial Modbus Broadcast for the TCP/IP server.
  4. Enter a Server Connection Idle Time in seconds, if enabled.
  5. Select the required TCP/IP client values for Client Connection Timeout and Client Message Timeout.
  6. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.