DOCA0036EN-14

Installing a 3G Modem on the Com’X

You can install a 3G modem on the Com’X.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must only be installed and serviced by qualified personnel.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462 or applicable local standards.
Failure to follow these instructions will result in death or serious injury.
  1. Power off the Com’X.
  2. Open the Com’X front door.
  3. Connect the 3G modem.
    • For modems that mount inside the Com’X, connect the modem to the internal USB port.
    • For 3G modems that do not mount inside the Com’X front cover, break off the tab to create an opening for the cable, then connect the modem cable to the internal USB port.
  4. Close the Com’X door as shown above.
  5. Power on the Com’X. The Radio Modem LED flashes to show the modem has been detected.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.