DOCA0036EN-14

Selecting a Network Configuration

Select the appropriate network configuration for your system.
  1. Click Settings > General Settings > Network Settings.
  2. Select the network configuration in the Choose your network configuration drop-down list.
  3. If necessary, enter the parameters for each connection interface displayed. Refer to the corresponding sections.
  4. Click Save changes.
  5. Wait for the Com’X to reboot.

    The power LED turns green when the reboot is complete.

** Configuring the Ethernet Ports, GPRS Settings, andConfiguring a Wi-Fi Network (see Reboot Cases)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.