DOCA0036EN-14

Configuring Warning Banner Settings

To configure Warning Banner settings:
  1. Navigate to Settings >Firewall Management.
  2. Click Warning Banner Settings.
  3. Click Yes to enable warning banner.
  4. Enter text to be displayed in the warning banner.
  5. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.