DOCA0036EN-14

Creating a Status Custom Model

You can create a new status custom model.
  1. Click the Custom Library main tab.
  2. Click +Create on the lower left part of the page.

    The Create a custom model dialog opens.

  3. Enter the following settings:
    Field Setting
    Select model type Select Status from drop down menu.
    Create model

    Select the basis for the new custom model:

    • New
    • Based on a custom model

    <base model type> If you are basing the new custom model on an existing custom model, select the existing model on which the new model is based.
    Model name Enter the name of the new custom model, or accept the default name Status_Custom.
    Default value of commodity Select a default commodity that the new model measures.
    Default value of usage Select a default value for how the new model is used.
  4. Click Create.

    The dialog closes, and the newly created custom model properties page opens for initial configuration.

  5. Configure the signal properties of Status custom model.

    Signal Properties

    Field

    Description

    Signal element

    Select the required signal element from the drop down menu.

    Value for 0

    Select the signal element state represented by the value 0 or accept the default value given.

    Value for 1

    Select the signal element state represented by the value 1 or accept the default value given.

  6. Click Save changes to save the configured Status custom model.
The custom signal element is selected for logging and publishing by default.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.