DOCA0036EN-14

Connecting a Standard Main Meter (Upstream Device)

You can connect the contact outputs from the properties area of the upstream device.
  1. Click the Device Settings main tab.
  2. Select the upstream device in the device tree view.
  3. Click the Digital and analog inputs collapsible menu.
  4. Select the name of the main meter in the Device drop-down list.
  5. Select the contact output that has to be connected in the Connector drop-down list.
  6. Click Save changes.

    The device tree view shows that the standard main meter is connected to an additional digital input.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.