DOCA0036EN-14

Connecting a Standard Main Meter (Main Meter)

You can connect the contact outputs from the properties collapsible menu of the standard main meter.
  1. Click the Device Settings main tab.
  2. Select the main meter in the device tree view.
  3. Select Pulse Output 1 in the Properties collapsible menu.
  4. Select the number of digital outputs in the drop-down list.
  5. Repeat steps 3 and 4 for the Pulse Output 2 properties.
  6. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.