DOCA0036EN-14

Creating a Custom Pulse Meter

You can create a customized pulse meter by inputting customized settings.
  1. Click the Custom Library main tab.
  2. Click +Create on the lower left part of the page.

    The Create a custom model dialog opens.

  3. Enter the following settings:
    Field Setting
    Select model type Select Pulse Meter.
    Create model

    Select the basis for the new custom model:

    • New
    • Based on a Schneider Electric model
    • Based on a custom model

    **angle brackets
    <base model type>
    If you are basing the new custom model on an existing Schneider Electric model or a custom model, select the existing model on which the new model is based.
    Model name Enter the name of the new custom model, or accept the default name Pulse Meter_Custom.
    Default value of commodity Select a default commodity the new model measures.
    Default value of usage Select a default value for how the new model is used
  4. Click Create.

    The dialog closes, and the newly created custom model properties page opens for initial configuration.

  5. Configure the measure properties for a newly created custom pulse meter model.

    The measure properties include the following:

    Field Description
    Count element Select a measure element from the list, or select Custom and type a personalized name into the Custom count element field.
    Count unit Select a measure unit from the list, or select Custom and type a personalized unit into the Custom count unit field.
    Pulse weight The pulse counter increases by this value each time a pulse is received. The list is restricted to the values that correspond to the selected meter type.
    Upper Range

    Defines when the active energy counter rolls back to zero.

    Flow element Select a flow element from the list, or select Custom and type a personalized name into the Custom flow element field.
    Flow unit Select a flow unit from the list, or select Custom and type a personalized unit into the Custom flow unit field.

Measurements table

The measure property selections you make, including customized properties, are reflected in the measurementstable.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.