DOCA0036EN-14

Defining a Modbus Custom Slave

After you have created the new Modbus custom slave model, you can complete its definition in the Custom Library.

This procedure requires that you have created a custom model.

  1. Select the new model in the model tree view, then click the Slave collapsible menu.
  2. Select the reading order in the Endianness drop-down list.

    This setting describes the register order to be used when a variable is formatted with more than one register.

    NOTE: The endianness depends on the device and must be selected in the Com’X settings. For example, PM700 is big endian and PM800 is little endian. The endianness setting is not used if variables are formatted with 16-bit registers.

  3. Click New frame.
consider making reference topic, needs short desc.

Modbus Custom Slave Register Examples

Register Register Number Read/write Scale Unit Format Interval Description
1037 1 R x1 kW INT +/–0...32767 Total active power
1041 1 R x1 kVAR INT +/–0...32767 Total reactive power
1049 1 R x1000 None INT –1000...1000 Total power factor
1054 1 R x10 Hz INT 0...4000 System frequency

When reading the device documentation, it appears that all variables can be read with 1 frame of registers (Function code 03) starting from register 1037 and ending with register 1054 (count = 18).

Continue to Creating a Modbus Frame to define a new frame.
**Creating a Modbus Frame related link
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.