DOCA0036EN-14

Exporting One or More Custom Models

You can export custom models.
  1. Click the Custom Library main tab.
  2. Navigate to the model you want to export. Either:
    • Click Models in the navigation tree to display a list of all models, or
    • Click Models, then <Model Type> (for the model type you wish to export).
  3. Do one of the following. Either:
    • To export a single model, click the Export icon () in the row for the model you want to export, or
    • To export multiple models, place a check mark next to the models you want to export, then click Export.
    The exported model is wrapped in a .zip file and sent to the default download location of your browser.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.