DOCA0036EN-14

Modifying a Custom Model

You can modify the settings of an existing custom model.
  1. Click the Custom Library main tab.
  2. Display a list of existing models. Either:
    • Click Models in the navigation tree to display a list of all models, or
    • Click Models, then <Model Type> (for the model type you wish to modify) to display a list of models of the selected type.
  3. Click the model in the list you want to modify.
  4. Make your edits of the configurable properties for the selected model.
  5. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.