DOCA0036EN-14

Deleting a Custom Model

You can only delete a model if no devices have been created from the model.
  1. Click the Custom Library main tab.
  2. Display a list of existing models. Either:
    • Click Models in the navigation tree to display a list of all models, or
    • Click Models, then
      **angle brackets
      <Model Type> (for the model type you wish to delete) to display a list of models of the selected type.
  3. Do one of the following. Either:
    • To delete a single model, click the delete icon () in the row for the model you want to delete, or
    • To delete multiple models, place a check mark next to the models you want to delete, then click Delete.
    A model is deleted when you issue the delete command. No message box appears and asks you to confirm the delete command.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.