DOCA0036EN-14

Connecting Devices to WT4200 Modbus Receiver

The WT4200 Modbus Receiver is a Modbus interface between the Com’X and the WT4200 radio transmitters.

Each transmitter is seen as a different channel for the WT4200 Modbus Receiver.

You must configure the WT4200 Modbus Receiver before adding it to the Com'X device list and connecting transmitters. WT4200 configuration determines to which channel the transmitter can be added. Refer to the PowerLogic WT4100 series / WT4200 series long-range RF wireless devices user manual for wireless receiver programming instructions.

WARNING
Inaccurate data results
The configuration in the Com’X must be consistent with the configuration in the WT4200 Modbus receiver.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

  1. Click the Device Settings main tab.
  2. Click the WT4200 in the device tree view.
  3. In the Channel collapsible menu, select the channel (C1, C2, and so on) to which the device is connected. Click the header to expand the channel area.
  4. Select Create a new device in the appropriate digital input dropdown list.
  5. Select the type of device to be created from the dropdown list.

    Only the devices that can be connected to this interface are listed. You may need to create your own custom device.

  6. Configure the device. Refer to the sections that correspond to the specific device category.
  7. Click Create and the device appears in the device tree view downstream from the WT4200.
** (see Custom Library) (see Devices That Can Connect to Digital Inputs)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.