DOCA0036EN-14

Discovering Zigbee Devices

With the ZigBee discovery function, the Com'X can discover ZigBee devices that are within range.

Do not launch the ZigBee discovery mode of several Com’X devices simultaneously. If you have two or more ZigBee networks in discovery mode, the ZigBee devices are installed randomly on these networks.

  1. Click the Com’X in the device tree view.
  2. Click Discover devices to open the Discovery window.
  3. Select the communication protocol ZigBee.
  4. Enter the Timeout time (in minutes).
  5. Click Start to discover the devices.
    In order to detect the ZigBee devices, you also need to activate the discovery mode on the different devices.

    Discovered devices are listed in the ZigBee Discovery window. Click Stop if you want to stop the ZigBee Discovery process.

  6. Close the ZigBee Discovery window.

    All the discovered devices appear in the device tree view. A Local ID is automatically assigned whenever a device is created. You can change the Local ID in Settings > Communication > Modbus Gateway > Device IDs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.