DOCA0036EN-14

Modifying a Device

You can modify device settings.
  1. Click the Device Settings main tab.
  2. Click the device in the device tree view.
  3. Modify the settings in the required collapsible menu.
  4. Click Save changes.
    NOTE: The device type cannot be modified. If a device is incorrectly configured, delete the device and create a new one.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.