DOCA0036EN-14

Selecting Measurements to Log or Publish

It is important to consider how much data is being logged across all devices when selecting the logging interval and number of topics to log.

Logging too many topics per interval may affect your Com’X performance, including degraded web page response and missed logging intervals. For example, for a logging interval of less than five minutes, it is recommended that you log no more than 8 devices with 50 total topics.

  1. Click the Device Settings main tab.
  2. Click the meter or sensor in the device tree view.
  3. Click the Measurements Table main tab.
  4. Select the Log check box of the measurement to be logged.
  5. Select the Publish check box to send the data to the selected publishing platform (optional).
  6. Click Save changes.
    Selecting Platform and Publication Frequency
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.