DOCA0036EN-14

Defining the Out of Service Time

You can define the Out of Service Time.
  1. Click Diagnostics > Communications Check.
  2. Select Yes for Enable Out of Service Time.
  3. Select the Out of Service Time. Options are 1, 2, 3, 4, 5, 10, 15, 30 and 60 minutes (default: 15).
  4. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.