DOCA0036EN-14

Executing a Manual Communications Check

In certain cases, you may not want to wait for the automated communications check interval and need to force the check to run manually.
  1. Click Diagnostics > Communications Check.
  2. Click Check Device Status to begin the check.
  3. Optionally, you can click Stop Status Check to stop the check.
The Status column displays In Service or Out of Service.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.