DOCA0036EN-14

Reading Device Registers

You can read Modbus registers from local and remote devices using Read Device Registers.
  1. Click Diagnostics > Read Device Registers
  2. Select a device from the Device Name drop-down list, or choose Select by Device ID for devices that aren't in the device list.
  3. If you chose Select by Device ID, enter the Local ID.

    If you selected a device name in the previous step, this field is populated automatically and cannot be changed.

    NOTE: The Slave ID is the identifier on the serial port to which it is connected. The Local ID is the identifier used by the Com’X.
  4. Enter a starting register and the number of registers to read.
  5. Select a data type.
  6. If you selected Holding or Input registers, choose a format for the returned data.
  7. Click Read.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.