DOCA0036EN-14

Viewing Statistics

You can view network or Modbus statistics.
  1. Click Diagnostics.
  2. Click one of the following categories:Network or Modbus.
  3. Click the expandable menu for the group of statistics you want to view.
  4. Click Refresh if you want to update the data.
    NOTE: Network statistics update approximately every 10 seconds.
** See Interpreting Statistics for a list of available parameters.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.