DOCA0036EN-14

Disabling DPWS and SSH services

DPWS and SSH services are enabled by default. DPWS uses a specific port for Com’X discovery and SSH uses a specific port for remote access by Schneider Electric technical support. For security reasons it is recommended to disable these services by setting the options to No and enabling them only when required.
NOTE: Com’X cannot be discovered by other devices after DPWS service is disabled. It is recommended to record the Com’X IP address before disabling DPWS service.

To disable DPWS and SSH services:

  1. Select Settings>Firewall Management>Services.
  2. Select No to disable DPWS service.
  3. Select No to disable SSH service.
  4. Select Save changes to save settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.