DOCA0036EN-14

Viewing the Measurements Table

The Measurements Table allows you to view all the meters and sensors of the system that log data. Only the data that has been selected for logging is present in the Measurements Table.
  1. Click the Measurements Table main tab.
  2. Select the required meters in the Filter by commodity field:
    • Click All to visualize all the commodities at the same time.
    • Click None to hide all the commodities at the same time.
    • Check the corresponding check box to view all the measurements of a commodity.
    • Uncheck the corresponding box to hide all the measurements of a commodity.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.