DOCA0036EN-14

Resetting to Factory Settings

When following the procedure below, all data and logs that have been stored are erased.
NOTICE
Hazard of IP address conflict
Disconnect the Com’X from any Ethernet networks before resetting the IP settings to factory values.
Failure to follow these instructions can result in impaired communications.

If you are using a Schneider Electric Service through DSP, contact Schneider Electric support before performing a factory reset. Otherwise, you must contact DSP support to reconnect to your subscribed service: dsp-support@schneider-electric.com.

To reset the energy server completely, follow this procedure to set all configuration settings to factory values:

  1. Power down the Com’X and wait until the power LED is off.
  2. Press simultaneously the Backup button and the Wi-Fi button on the Com’X front face and power up the Com’X.

    Hold the buttons until the power LED flashes three times.

  3. Release the buttons.

    It can take up to 20 minutes for the Com’X to reboot.

  4. Wait for the Com’X to restart completely.

    The power LED is:

    • orange when the Com’X is starting.

    • green when the Com’X has been reset to factory settings and is ready to be configured.

  5. Follow the instructions described in Access the User Interface to access the Com’X web pages.
** Access the User Interface
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.