DOCA0036EN-14

Restarting the Com’X from the Web Interface

Use the Restart Com'X feature to manually restart the Com’X.
  1. Click Maintenance > System Settings.
  2. Under Restart Com'X, click Restart, then Yes to confirm.

    The reboot begins.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.