DOCA0036EN-14

Saving the Configuration Locally

You can save the configuration locally.
  1. Click Maintenance > System Settings.
  2. Click Save Configuration OR Backup for Duplication in the Configuration Management collapsible menu.

    According to the web browser used, a dialog box appears to open, save, or cancel the configuration file.

  3. Select the option to save the file in the dialog box.

    The date and time of the last configuration backup are displayed under the Save Configuration button.

  4. In the Choose File field, select the location on the computer to save the file and save the configuration.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.