DOCA0036EN-14

Upgrading Firmware via DSP

Firmware upgrade through DSP is managed by Schneider Electric technical support.

At the end of the firmware upgrade process, the Com’X reboots. Logging and publication restart automatically.

NOTE: It is not recommended to make the first firmware upgrade of the Com’X using the DSP through GPRS connection. Because the GPRS connection has a speed of only 20 kb/s, the firmware update could take several hours.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.