DOCA0036EN-14

Quickstart: Setting up and Starting Data Logging

Below are the general tasks related to starting data logging. There may be additional steps for publishing to a specific platform.
  1. Add the downstream devices as in Adding a Downstream Device. There are additional configuration tasks for each type of device:
  2. Select the measurements to log as in Selecting Measurements to Log or Publish
  3. Define the logging interval as in Defining the Logging Intervals
  4. Start the data logging as in Starting the Data Logging
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.