DOCA0036EN-14

Quickstart: Viewing On-board Data

You can view real time and logged data on the Com’X 210 without having to connect to a hosted platform. Below are the steps for viewing on-board data.
  1. Add the downstream devices as in Adding a Downstream Device. There are additional configuration tasks for each type of device:
  2. Complete the following steps to view an Energy dashboard. Skip to step 3 to view real time data.
  3. View real time data that has been selected for logging: Viewing the Measurements Table
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.