DOCA0036EN-14

Creating a Contact

You can create a contact.
  1. Click Settings > General Settings > Contact Management.
  2. Type the Name and Email address, then press Enter or click +.
    The Contact is added to list.
  3. Click Save Recipient List.

The contacts are now available in:

  • Publication settings for publishing over SMTP.
  • Custom Events for setting up email on events.

To delete a contact, click the X beside the contact name, then Save Recipient List.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.