DOCA0036EN-14

Disabling the Password Reset Button

For a Com’X installed in a publicly accessible location, you can disable the password reset function for the Backup button.

The Backup button () is located on the front face.

If you lose the default admin password, you must perform a factory reset on the Com’X to reset the password to default. This destroys all logged data, user accounts, and configuration.

NOTICE
IRRECOVERABLE PASSWORD
Record your device's user and password information in a secure location.
Failure to follow these instructions can result in data loss.

It is recommended to save a backup configuration before disabling the password reset button.

  1. Click Settings > Security > Firewall Management.
  2. Click Enable default admin reset.
  3. Click No to disable the password reset button.
  4. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.