DOCA0036EN-14

Enabling Schneider Electric Services

To enable Schneider Electric Services:
  1. Configure Proxy Settings, if required.
  2. Click Settings > General Settings > Schneider Electric Services.
  3. Click Yes in the Configuration section.
  4. Click Save Changes.

All three states display in green and a confirmation message displays when DSP connection is enabled.

NOTE: The configured date and time are synchronized periodically and display after DSP sync time command runs automatically.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.