990-91274E-001

Unpack the Cabinet

  1. Remove the indicated bolts.
  2. Lift up the cabinet with a forklift and remove the pallet parts.
  3. Lower the cabinet to the floor and remove the indicated bolts.

    700 mm Wide Classic Battery Cabinet

    1000 mm Wide Classic Battery Cabinet

  4. Remove the wooden plates.
QR code for this page

Was this helpful?