990-6287B-001

Configure the Network Settings

  1. From the home screen of the display select Settings > General settings > Network .
  2. Set the Device ID for communication using the left and right arrows. Choose between 1-255.
  3. Set the Baud rate for communication using the left and right arrows. Choose between 2400, 4800, 9600, 14400, and 19200.
  4. Tap Save settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?