990-5992E-001

Install the Optional IP30 Kit (E3MOPT009)

  1. Remove the bottom plate from the rear side of the UPS. Save for reinstallation.
  2. Remove the top plate from the rear side of the UPS. Dispose of the plate and save the screws for reinstallation of the IP30 top plate.
  3. Install the top plate provided with the IP30 kit on the rear side of the UPS.
  4. Reinstall the bottom panel on the rear side of the UPS or save for installation after power cable connection.
QR code for this page

Was this helpful?