990-5992E-001

Overview of Parallel System

NOTE: In parallel systems with an external maintenance bypass breaker Ext. MBB, the maintenance bypass breakers MBB must be padlocked in the open position.

UPSs for External Batteries

MIB Mains input breaker
BIB Bypass input breaker
UIB Unit input switch
SSIB Static switch input switch
UOB Unit output switch
Ext. UOB External unit output breaker
MBB Maintenance bypass switch
Ext. MBB External maintenance bypass breaker
SIB System isolation breaker
BB Battery breaker
QR code for this page

Was this helpful?