990-5992E-001

Remove the UPS from the Pallet

  1. Move the UPS to the final installation area using a forklift.
  2. Remove the shipping materials and the ramp from the UPS.
  3. Loosen the bolts and remove the shipping brackets. Save the bolts for the ramp and dispose of the shipping brackets.
  4. Place the ramp on the pallet and fasten with the bolts from the shipping bracket.
  5. Roll the UPS down from the pallet.
  6. Move the UPS to its final location and use a wrench to lower the levelling feet. Ensure that the cabinet is level.
  7. Lock the wheels.
QR code for this page

Was this helpful?